This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Wifi interference detection?



Two questions regarding the Wifi interference.

1. Energy detection will scan all channels, I think the time per channel scan is around 0.5s, could we extend this scanning time?

2. Regarding CSMA/CA in MAC layer, channel sense will sense the dB energy level(can check wifi traffic)? or it only sense the busy 802.15.4 traffic(can not check wifi traffic).  I remember we can configure in zstack?

Thanks

Rui