Other Parts Discussed in Thread: Z-STACK
Hi,
I want to increase the Radio range in run time by calling ZMacSetTransmitPower(). But I don't know what is the default dB is for sampleLight or SampleSw where it is defined. But I want to increase it to 3dB. ZMacSetTransmitPower(TX_PWR_PLUS_3).
My aim is to get good range with less/ Zero PER while data Exchanging, Child should not be out of range after it joined and fixed in particular place.
Since Tx power will affect the battery, so my plan to change the Tx power depends on RSSI or LQI value.
Question 1:
If I set Tx Power as 3dB in zcl_xxx_init. It will increase the range of beacon request also for searching it's parent or that is only applicable after it's joins to network?
Question 2:
I know I will get the rssi value through afIncomingMSGPacket_t. If I send a data from End device to Coordinator, then Coordinator will know the End device RSSI value. But how End device will come know it's own RSSI value.
Question 3:
What is the difference between RSSI and LQI value. which will indicate the radio power and how I will come to know the signal is weak.