Other Parts Discussed in Thread: CC2538, CC1310
Hello,
I used the SmartRF06 Evaluation Board with SmartRF Studio 7.2 and I'm no longer able to communicate with the board. The equipment worked the first time I connected it to SmartRF. I only noticed the issues the next time I went to use the board. The red LED for advanced mode is on, though it doesn't look fully lit.
I've tried connecting it to SmartRF Studio but I get a message stating it has an existing flash. I select OK to delete the flash then SmartRF crashes.
I've connected it to Flash Programmer 2 to delete the flash and I get the following message.
I tried Forced mass Erase but after initiating access to the target I get the following failure messages:
Create XBAL Object failed: Board reset before connect failed
Failed to create device object.
When uploading the program in Code Composer 6 I get the following message.
Anyone know what I can do to get the board functional again?
Thank you,
Juan