Hi all,
I am using Z stack on CC2538 and is using 2.4GHz (Worldwide,I am from India).In my country only 2.4GHz is supported .So can i use other frequeny bands(915MHz and 868MHz)
If i pass the channels corresponding to these frequencies(915MHz and 868MHz) network is not forming.
So is it possible to use other two frequencies for testing purpose in india.
Or is it like that zstack or board (cc2538) radio is configured to support only 2.4ghz.
Thanks
Amit Kumar