i'm curious if there is any ready-made hardware/software-solution for using the TCP socket connection of ZTool?
i guess the intended use is to remotely connect ZTool to a device over LAN instead of UART, but is there any solution provided by TI (for example using the TivaC TM4C1294 connected Launchpad or anything similar with LAN connection) or is it up to the user to build its own hardware (e.g. using a separate Uart-to-TCP-Bridge connected to the Uart-enabled ZigBee-Node)?
It is a helpful debug-feature to connect ZTool to devices that are farther away and only reachable over network-connection. I'm sure somebody of the ZTool-developers already used this and it would be nice to share some more information about it.
Thanks, Albert