Hello:
I'm using the Zigbee ZStack-CC2530-2.3.0-1.4.0 with IAR workbench 8051 and SmartRF Flash Programmer to program a module CC2530F2530. I want to program the ESP coordinator application of Smart energy profile in this device but, when I want the program the .hex file (intel-extended) in flash, appear the next error:

I don't know why, because I'm using the original Smart energy profile application and when I build the code I have the next report:
________________________________________________________________
IAR Universal Linker V4.61T/W32
Copyright (C) 1987-2010 IAR Systems AB.
176 825 bytes of CODE memory
18 bytes of DATA memory (+ 83 absolute )
7 615 bytes of XDATA memory
192 bytes of IDATA memory
8 bits of BIT memory
697 bytes of CONST memory
Errors: none
Warnings: none
Total number of errors: 0
Total number of warnings: 1
___________________________________________________________________
I have enough space to program this code in CC2530F256 flash memory.
Please, if someone has the same problem and can solved please replay.
Best regards
NAlves