Hi,
I am using CC2530 as my ZCD and I have Zigbee Curtain Controller which is added with ZCD. Now I am trying to control the Curtain controller through Z-tool application with below mentioned parameters.
For your reference:
<TX>10:59:12.03 COM5 AF_DATA_REQUEST (0x2401)
DstAddr: 0x09CA
DestEndpoint: 0x01
SrcEndpoint: 0x07
ClusterID: 0x0102
TransID: 0x01
Options: 0x02
Radius: 0x07
Len: 0x03
Data: ... (0x01, 0x01, 0x00)
1) Now I want to control the percentage in Curtain Controller, what command should I use for it.
Thanks & Regards
Pavithran J