Other Parts Discussed in Thread: CC2531, Z-STACK
Hi,
Currently I'm trying to build a Zigbee network using the CC2530 as a ZC. I'm just getting to know zigbee and so far it seems to be quite different from BLE or other low power wireless interfaces.
The mentioned CC2530 module has the Z-Stack 3.0.2 ZNP firmware flashed and is connected to the pc which runs Z-Tool 2.0. I have a thermostat which is the device i'm trying to interface with. Beside this i have a CC2531 module connected as sniffer on my pc.
I have successfully paired the device, requested descriptors and can bind to clusters. However, I'm expecting data when I bind to a specified cluster but nothing is showing up. I have the Z-Tool log with the commands sent after pairing noted below.
Some details on addresses:
Coordinator IEEEAddr: 0x00124B001D37AA40
Device NwkAddr: 0xD1A3
Device IEEEAddr: 0x842E14FFFE590A49
<TX>10:17:15.63 COM19 ZDO_ACTIVE_EP_REQ (0x2505) DstAddr: 0xD1A3 NWKAddrOfInterest: 0xD1A3 <RX>10:17:15.64 COM19 ZDO_ACTIVE_EP_REQ_SRSP (0x6505) Status: afStatus_SUCCESS (0x0) <RX>10:17:18.86 COM19 ZDO_ACTIVE_EP_RSP (0x4585) SrcAddr: 0xD1A3 Status: ZDP_SUCCESS (0x0) NwkAddr: 0xD1A3 ActiveEPCount: 0x01 ActiveEPList: . (0x01) <TX>10:20:30.93 COM19 ZDO_SIMPLE_DESC_REQ (0x2504) DstAddr: 0xD1A3 NWKAddrOfInterest: 0xD1A3 Endpoint: 0x01 <RX>10:20:30.94 COM19 ZDO_SIMPLE_DESC_REQ_SRSP (0x6504) Status: afStatus_SUCCESS (0x0) <RX>10:20:31.24 COM19 ZDO_SIMPLE_DESC_RSP (0x4584) SrcAddr: 0xD1A3 Status: ZDP_SUCCESS (0x0) NwkAddr: 0xD1A3 Len: 0x1C Endpoint: 0x01 ProfileID: 0x0104 DeviceID: 0x0301 DeviceVersion: 1 (0x1) NumInClusters: 0x08 InClusterList: 0x0000, 0x0001, 0x0003, 0x000A, 0x0020, 0x0201, 0x0204, 0x0B05 NumOutClusters: 0x02 OutClusterList: 0x0000, 0x0019 <TX>10:27:08.58 COM19 AF_REGISTER (0x2400) EndPoint: 0x01 AppProfID: 0x0104 AppDeviceId: 0x0301 AppDevVer: 0x01 LatencyReq: NO_LATENCY_REQS (0x0) AppNumInClusters: 0x08 AppInClusterList: 0x0000, 0x0001, 0x0003, 0x000A, 0x0020, 0x0201, 0x0204, 0x0B06 AppNumOutClusters: 0x02 AppOutClusterList: 0x0000, 0x0019 <RX>10:27:08.59 COM19 AF_REGISTER_SRSP (0x6400) Status: afStatus_SUCCESS (0x0) <TX>10:44:23.66 COM19 ZDO_BIND_REQ (0x2521) DstAddr: 0xD1A3 SrcAddress: 0x842E14FFFE590A49 SrcEndpoint: 0x01 ClusterID: 0x0000 BindAddrMode: 0x03 (ADDRESS_64_BIT) (0x3) BindAddr: @.7..K.. (0x40, 0xAA, 0x37, 0x1D, 0x00, 0x4B, 0x12, 0x00) BindEndpoint: 0x01 <RX>10:44:23.67 COM19 ZDO_BIND_REQ_SRSP (0x6521) Status: afStatus_SUCCESS (0x0) <RX>10:44:28.82 COM19 ZDO_BIND_RSP (0x45A1) SrcAddr: 0xD1A3 Status: ZDP_SUCCESS (0x0) |
After these command's, no data is showing up. Is there any invalid config that can be seen? Or am I misunderstanding the way Zigbee handles data?
Best regards