Other Parts Discussed in Thread: CC2530-CC2591EM
Hello team,
My Customer would like to know if the CC2430-CC2591EMK device meets the EN 300 328 v2.2.2 ?
Regards,
Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
My Customer would like to know if the CC2430-CC2591EMK device meets the EN 300 328 v2.2.2 ?
Regards,
Renan
Hi Renan,
While I don't have information about that exact combination, I do know that the CC2530-CC2591EM Reference Design, which from an RF perspective, is very similar. The app note here has a section on regulatory information, where it says that it passes FCC, which is typically stricter than EN 300 328. You may have to adjust the power settings though as the note says. The 2430 is also NRND, so I'd recommend designing with the 2530 if this is the route you're looking to go down.
Best,
Nate