In file "sbl_device_cc2652.h", there is defined "#define SBL_CC2652_RAM_SIZE_CFG 0x40082250". But in swcu185d, the Register 0x40082250 is not RAM SIZE.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In file "sbl_device_cc2652.h", there is defined "#define SBL_CC2652_RAM_SIZE_CFG 0x40082250". But in swcu185d, the Register 0x40082250 is not RAM SIZE.
Hey Aries,
Looking further into SWCU185, 0x40082250 points to the reserved location after PRCM:RAMRETEN for memory retention control. That makes it harder for a developer to ascertain as compared to SBL_CC2652_FLASH_SIZE_CFG which is 0x4003002C from the FLASH:FLASH_SIZE register. Are you experiencing any issues with using the bootload tool for your CC2652R7 device?
Regards,
Ryan
Now I'm testing on CC2652R1 not CC2652R7. The register 0x4003002C can get the quantity of pages of Flash ROM. But 0x40082250 have no meaning.
I see your point. SBL_CC2652_RAM_SIZE_CFG doesn't appear to be used by sblAppEx and could be a deprecated value from the CC26X0. There does not appear to be an equivalent accessible register for reading the SRAM size.
Regards,
Ryan