This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530-CC2592EM-RD: S11 of CC2530+CC2592

Part Number: CC2530-CC2592EM-RD
Other Parts Discussed in Thread: CC2592, CC2530

I want to test the S11 of CC2530+CC2592 RF TX and RX chain.

Use SmartRF Studio 7 to set TX or RX mode for CC2530+CC2592, how to confirm if CC2592 is working at a right mode (TX=PA mode, RX=LNA mode) ?

Connection status:

CC2530 P1.1  connect to CC2592 PA_EN

CC2530 P1.3  connect to CC2592 LNA_EN

CC2530 P0.7  connect to CC2592 HGM