Hi,
I try to get sniffer log in Packet Sniffer using CC2531 USB log
I set the Channel in 13
no response o the log Screen
I couldn't find the issue. can you help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I try to get sniffer log in Packet Sniffer using CC2531 USB log
I set the Channel in 13
no response o the log Screen
I couldn't find the issue. can you help me.
I know you set it to channel 13 but do you have any Zigbee device sending message on channel 13?
Which example do you run as Zigbee devices? By the way, most of Zigbee device would use channel 11 so maybe you can sniff channel 11 to see if there is any packet.
I need to get zigbee on/off , dimmer, curtain modules .
I set the channel in 11 but no any packet.
What is your coordinator? Do you use Ztool+ZNP to act as coordinator to form Zigbee network?
Do you use Zigbee 3.0? If so, you can refer to steps in https://sunmaysky.blogspot.com/2017/02/use-ztool-z-stack-30-znp-to-set-up.html to setup coordinator to work on channel 13 and use sniffer to check packet in channel 13 at the same time.