This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538: Is there any way to Remove or Delete specific endpoint from zigbee network.

Part Number: CC2538
Other Parts Discussed in Thread: Z-STACK

Hello Community,

I am working on the CC3538 Zigbee devices with Zigbee Linux Gateway Application.

Some of our devices support multiple endpoints.

Deleting the device from the network will remove all the associated devices connected to individual endpoints from the network.

Instead, I want to remove only a specific endpoint from the network without removing the actual device from the network.

Is that possible?

If yes, Please guide me on how can I do that?

regards,

Shiv Patil.