Hi
I'm using LPSTK-CC1352 with simplelink_cc13xx_cc26xx_sdk_5_30_01_01 with thermostat_CC1352R1_LAUNCHXL_tirtos_ccs example.
Below you can see 12 devices connected to Border Router.
| Role | RLOC16 | Age | Avg RSSI | Last RSSI |R|D|N| Extended MAC |
+------+--------+-----+----------+-----------+-+-+-+------------------+
| R | 0x0c00 | 5 | -76 | -76 |1|1|1| aa32c2218c33d125 |
| R | 0x1000 | 1 | -76 | -76 |1|1|1| 96b99ca7b1cbcef0 |
| R | 0x1c00 | 4 | -53 | -54 |1|1|1| 12bfc0fe903ab8eb |
| R | 0x2400 | 2 | -70 | -71 |1|1|1| 4a13e4cb6aba20a7 |
| R | 0x3000 | 0 | -64 | -64 |1|1|1| 22514403ff548850 |
| R | 0x3800 | 1 | -70 | -70 |1|1|1| 8e2c008048112bcf |
| R | 0x4400 | 1 | -67 | -67 |1|1|1| dec0d636bb2724cd |
| R | 0x4800 | 1 | -58 | -59 |1|1|1| beaf7eb8cde9d8e1 |
| R | 0xa400 | 0 | -66 | -67 |1|1|1| cea80d3d00dae0a1 |
| R | 0xbc00 | 2 | -80 | -81 |1|1|1| ced8512fde5af960 |
| R | 0xe000 | 1 | -66 | -67 |1|1|1| 82fe20342215f694 |
| R | 0xf400 | 1 | -63 | -63 |1|1|1| 8aa54ebf43877335 |
Its quite confusing that LQ out is very small for all devices in comparison to LQ in. It looks very assymetrical and make impression like Input path has some path with additional attenuation or is not configured well.
I'm using standard example. Beagle Bone is equipped with Nordic nRF52840 dongle with set 8dBm output power. Shall I make any custom configuration for standard thermostat_CC1352R1_LAUNCHXL_tirtos_ccs example used with LPSTK-CC1352 ?
| ID | RLOC16 | Next Hop | Path Cost | LQ In | LQ Out | Age | Extended MAC | Link |
+----+--------+----------+-----------+-------+--------+-----+------------------+------+
| 3 | 0x0c00 | 63 | 0 | 3 | 1 | 1 | aa32c2218c33d125 | 1 |
| 4 | 0x1000 | 63 | 0 | 3 | 1 | 0 | 96b99ca7b1cbcef0 | 1 |
| 7 | 0x1c00 | 56 | 1 | 3 | 2 | 1 | 12bfc0fe903ab8eb | 1 |
| 9 | 0x2400 | 63 | 0 | 3 | 1 | 2 | 4a13e4cb6aba20a7 | 1 |
| 12 | 0x3000 | 63 | 0 | 3 | 1 | 6 | 22514403ff548850 | 1 |
| 14 | 0x3800 | 56 | 1 | 3 | 1 | 3 | 8e2c008048112bcf | 1 |
| 17 | 0x4400 | 63 | 0 | 3 | 1 | 0 | dec0d636bb2724cd | 1 |
| 18 | 0x4800 | 63 | 0 | 3 | 1 | 0 | beaf7eb8cde9d8e1 | 1 |
| 41 | 0xa400 | 56 | 1 | 3 | 1 | 6 | cea80d3d00dae0a1 | 1 |
| 47 | 0xbc00 | 63 | 0 | 2 | 1 | 8 | ced8512fde5af960 | 1 |
| 51 | 0xcc00 | 63 | 0 | 0 | 0 | 0 | 0000000000000000 | 0 |
| 56 | 0xe000 | 7 | 1 | 3 | 2 | 0 | 82fe20342215f694 | 1 |
| 61 | 0xf400 | 63 | 0 | 3 | 1 | 0 | 8aa54ebf43877335 | 1 |