This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SIMPLELINK-CC13X2-26X2-SDK: Cannot set MAX_RTG_SRC_ENTRIES higher than 255

Part Number: SIMPLELINK-CC13X2-26X2-SDK
Other Parts Discussed in Thread: SYSCONFIG, Z-STACK

I'm trying to configure a MAX_RTG_SRC_ENTRIES higher than 256 but this always fails with the following error:

I event tried forcing "srcRtgTableIndex_t" to be an uint16_t with the following changes, but the error is still the same:

Something I find very suspicious is that the error contains the path: "C:\.conan\ac47fe\1\source\ti\zstack\stack\nwk\nwk_globals.h". Since I'm compiling on Mac, which doesn't have a C: drive this cannot be true (and indicates to me it isn't using the nwk_globals.h from my SDK location).