How do I output the receiver sync signal on a GPIO pin?
In section 25.3.2.8 (External Signaling) of the TRU, it states:
...The signal RATGPO1 may be configured
to go high when sync is found in the receiver, and low when the packet is received or reception aborted
(this does not work for the IEEE 802.15.4 receiver command). To map RATGPO1 to a RFC_GPO signal, an
additional override is needed....
Given that I am using 802.15.4, how can this be done?
Thanks!