Other Parts Discussed in Thread: CC2530EMK, MSP-EXP430FR5739, CC-DEBUGGER, CC2530EM, CC2530, CC2500
I want to use a CC2530EMK with the ZigBee protocol but don't want to get the IAR compiler. I had read in the forms that I could use the ZStack-ZAP-MSP430-1.0.4 download swrc173.zip from http://www.ti.com/tool/z-stack. Every time I tried to download the file it said the file was not available for download. I noticed the current version is 2.5 and figured that it may be obsolete. I was able to download the ZStack-CC2530-2.5. I did see a ZNP hex file in \Projects\zstack\ZPN\CC253x\bin\ directory called CC2530ZNP-SB.hex. Is this the correct file to program the CC2530EMK with if I want to control it from a MSP430 through SPI?
Another question I have is if I can program the CC2530EMK with either the MSP-EXP430F5529 or the MSP-EXP430FR5739? If so do I use the SmartRF FLASH Programmer swrc044m.zip or is there a document on how to do this? If not what would be a good low cost method of doing this?