Other Parts Discussed in Thread: Z-STACK
Tool/software:
Hello,
I am currently working on a Zigbee application using the Z-Stack and encountered an issue while sending a Config Reporting command from a coordinator to an endDevice.
The configuration is successfully received on the endDevice. However, when the BDB_FINDING_BINDING_CAPABILITY_ENABLED option is disabled, the Z-Stack fails to save the configuration. Upon analyzing the code in bdb_reporting.c, specifically in the function bdb_ProcessInConfigReportCmd, I found that it fails due to the absence of an endPointDescriptor. The issue is located in this part of the code:
// Find Ep Descriptor
endPointDesc_t* epDescriptor = bdb_FindEpDesc(pInMsg->endPoint);
if (epDescriptor == NULL)
{
return (ZInvalidParameter);
}
The problem seems to stem from the
bdb_HeadEpDescriptorList pointer, which is not initialized when BDB_FINDING_BINDING_CAPABILITY_ENABLED is disabled. In the file af.c, within the function afRegisterExtended, I noticed that the initialization of bdb_HeadEpDescriptorList is conditioned by this option:#if (BDB_FINDING_BINDING_CAPABILITY_ENABLED == 1)
// Make sure we add at least one application endpoint
if ((epDesc->endPoint != 0) && (epDesc->endPoint < BDB_ZIGBEE_RESERVED_ENDPOINTS_START))
{
bdb_HeadEpDescriptorList = epList;
ep->epDesc->epType = bdb_zclFindingBindingEpType(ep->epDesc);
}
#endif
To resolve this issue, I modified the code to initialize
bdb_HeadEpDescriptorList even when BDB_FINDING_BINDING_CAPABILITY_ENABLED is disabled. Here is the updated code:// Make sure we add at least one application endpoint
if ((epDesc->endPoint != 0) && (epDesc->endPoint < BDB_ZIGBEE_RESERVED_ENDPOINTS_START))
{
bdb_HeadEpDescriptorList = epList;
#if (BDB_FINDING_BINDING_CAPABILITY_ENABLED == 1)
ep->epDesc->epType = bdb_zclFindingBindingEpType(ep->epDesc);
#endif
}
With this modification, the reporting configuration works correctly, and the Z-Stack successfully saves the configuration.
My question is: why is the initialization of bdb_HeadEpDescriptorList conditioned by BDB_FINDING_BINDING_CAPABILITY_ENABLED in the original Z-Stack? This logic seems to block basic features like reporting when this option is disabled. Is there a specific reason for this design, or are there implications I should be aware of?
Thank you in advance for your insights!