This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Whether the zigbee direct function is supported in the SDK simplelink_lowpower_f3_sdk_8_20_00_119

Part Number: CC2340R5


Tool/software:

I found that CC2340 runs the ZBOSS protocol stack.

ZBOSS supports the following Zigbee Direct roles and services:

  • Zigbee Direct Device (ZDD). ZDD has both an IEEE 802.15.4 radio and a

Bluetooth Low Energy radio, running BLE in a Peripheral role

  • Zigbee Virtual Device (ZVD). ZVD has at least BLE radio, running BLE in a

Central role

  • Zigbee Direct Security Service
  • Zigbee Direct Commissioning Service
  • Zigbee Direct Tunnel Service

So, does CC2340 support the above functions.