Hallo everybody,
just one little question. Is it possible to send AF data with the extended address instead of the short address as source address? The function call of
afStatus_t AF_DataRequest( afAddrType_t *dstAddr, endPointDesc_t *srcEP,
uint16 cID, uint16 len, uint8 *buf, uint8 *transID,
uint8 options, uint8 radius );
seems to not support such an option. Thanks in advance for your answers.
Regards,
Tobias