Other Parts Discussed in Thread: Z-STACK
I am new to z-stack and digging through the sample application, and try to understand how things work. right now, I am reading the temperature sensor, thermostat, and heating/cooling unit sample application in the z-stack Home 1.2. I am a little confused about how the input/out clusters are defined in the binding process using EZ mode and end-devince binding request.
In the sample temp sensor app, the code for end device binding is as follows:
// NOT ZCL_EZMODE, Use EndDeviceBind
static cId_t bindingOutClusters[] =
{
ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT
};
#define ZCLSAMPLETEMPERATURESENSOR_BINDINGLIST 1
// Initiate an End Device Bind Request, this bind request will only use a cluster list that is important to binding.
ZDP_EndDeviceBindReq( &dstAddr, NLME_GetShortAddr(), SAMPLETEMPERATURESENSOR_ENDPOINT,
ZCL_HA_PROFILE_ID, 0, NULL, ZCLSAMPLETEMPERATURESENSOR_BINDINGLIST, bindingOutClusters,FALSE );
And for EZ mode binding, the following is used:
static uint16 clusterIDs[] = { ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT }; // only bind on the Temperature Measurement cluster
// Invoke EZ-Mode
ezModeData.endpoint = SAMPLETEMPERATURESENSOR_ENDPOINT; // endpoint on which to invoke EZ-Mode
if ( ( zclSampleTemperatureSensor_NwkState == DEV_ZB_COORD ) ||
( zclSampleTemperatureSensor_NwkState == DEV_ROUTER ) ||
( zclSampleTemperatureSensor_NwkState == DEV_END_DEVICE ) )
{
ezModeData.onNetwork = TRUE; // node is already on the network
}
else
{
ezModeData.onNetwork = FALSE; // node is not yet on the network
}
ezModeData.initiator = TRUE; // Temperature Sensor is an initiator
ezModeData.numActiveInClusters = 1;
ezModeData.pActiveInClusterIDs = clusterIDs;
ezModeData.numActiveOutClusters = 0; // active output cluster
ezModeData.pActiveOutClusterIDs = NULL;
zcl_InvokeEZMode( &ezModeData );
In the simpledescriptor, the following is defined:
#define ZCLSAMPLETEMPERATURESENSOR_MAX_INCLUSTERS 3
const cId_t zclSampleTemperatureSensor_InClusterList[ZCLSAMPLETEMPERATURESENSOR_MAX_INCLUSTERS] =
{
ZCL_CLUSTER_ID_GEN_BASIC,
ZCL_CLUSTER_ID_GEN_IDENTIFY,
ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT
};
#define ZCLSAMPLETEMPERATURESENSOR_MAX_OUTCLUSTERS 1
const cId_t zclSampleTemperatureSensor_OutClusterList[ZCLSAMPLETEMPERATURESENSOR_MAX_OUTCLUSTERS] =
{
ZCL_CLUSTER_ID_GEN_IDENTIFY
};
For the thermostat, the following is defined:
#define ZCLSAMPLETHERMOSTAT_MAX_INCLUSTERS 3
const cId_t zclSampleThermostat_InClusterList[ZCLSAMPLETHERMOSTAT_MAX_INCLUSTERS] =
{
ZCL_CLUSTER_ID_GEN_BASIC,
ZCL_CLUSTER_ID_GEN_IDENTIFY,
ZCL_CLUSTER_ID_HVAC_THERMOSTAT
};
#define ZCLSAMPLETHERMOSTAT_MAX_OUTCLUSTERS 1
const cId_t zclSampleThermostat_OutClusterList[ZCLSAMPLETHERMOSTAT_MAX_OUTCLUSTERS] =
{
ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT
};
// NOT ZCL_EZMODE, Use EndDeviceBind
static cId_t bindingOutClusters[] =
{
ZCL_CLUSTER_ID_HVAC_THERMOSTAT
};
#define ZCLSAMPLETHERMOSTAT_BINDINGLIST_OUT 1
static cId_t bindingInClusters[] =
{
ZCL_CLUSTER_ID_HVAC_THERMOSTAT,
ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT
};
#define ZCLSAMPLETHERMOSTAT_BINDINGLIST_IN 2
ZDP_EndDeviceBindReq( &dstAddr, NLME_GetShortAddr(),
SAMPLETHERMOSTAT_ENDPOINT,
ZCL_HA_PROFILE_ID,
ZCLSAMPLETHERMOSTAT_BINDINGLIST_IN, bindingInClusters,
ZCLSAMPLETHERMOSTAT_BINDINGLIST_OUT, bindingOutClusters,
TRUE );
//invoke EZ mode
zclEZMode_InvokeData_t ezModeData;
static uint16 clusterIDs[] = { ZCL_CLUSTER_ID_HVAC_THERMOSTAT }; // only bind on the Thermostat cluster
// Invoke EZ-Mode
ezModeData.endpoint = SAMPLETHERMOSTAT_ENDPOINT; // endpoint on which to invoke EZ-Mode
if ( ( zclSampleThermostat_NwkState == DEV_ZB_COORD ) ||
( zclSampleThermostat_NwkState == DEV_ROUTER ) ||
( zclSampleThermostat_NwkState == DEV_END_DEVICE ) )
{
ezModeData.onNetwork = TRUE; // node is already on the network
}
else
{
ezModeData.onNetwork = FALSE; // node is not yet on the network
}
ezModeData.initiator = TRUE; // Thermostat is an initiator
ezModeData.numActiveInClusters = 0;
ezModeData.pActiveInClusterIDs = NULL;
ezModeData.numActiveOutClusters = 1; // active output cluster
ezModeData.pActiveOutClusterIDs = clusterIDs;
zcl_InvokeEZMode( &ezModeData );
Here are my questions:
- doc says to use EZ mode bind thermostat and temp sensor, but they are both initiators, shouldn't we bind a initiator and a target?
- in the sample temp sensor app, the ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT is in the output clusters for end-device binding, and in the input clusters list for EZ mode binding. Why is this?
- say we are binding thermostat and temp sensor, and they indeed can be paired. I suppose this works by matching ZCL_CLUSTER_ID_MS_TEMPERATURE_MEASUREMENT, in the input of temp sensor, and output in the thermostat. I can sort of understand how the ED binding works, but cannot seem to have a clue how it works in the EZ mode.
Thanks a lot for your help on my lengthy question.