This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RF Coverage of CC2538EM

Other Parts Discussed in Thread: Z-STACK

I did a simple outdoor test (line of sight) between two CC2538EM (+smartrf06eb) boards that has GenericApp of Z-Stack.

The default TX power is 0 dBm on the SW, and the datasheet says the receiver sensitivity is -97 dBm. I don't know what is the gain/loss of the on-board antenna and miss-match, but if I assume 4 dB on each side, I would expect to have >100 m coverage according to the path loss formula. However, the boards lost the link about 20 m distance. Is it normal to have coverage about 20m between two CC2538EM or do I miss something to take into the calculation?