This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Source code for TIDM-LOWEND-IHD CC2530 devices

Other Parts Discussed in Thread: TIDM-LOWEND-IHD, CC2530

Hello all,

I am working with the design files of the TIDM-LOWEND-IHD and I found here the HEX files for the CC2530 coordinator and end device that should be used with the IHD.  I programmed this files and could establish connection between them, but I can only send active power in one direction, from coordinator to end device.  I would like to use this code and send also other variables that I am measuring, but as I have no access to the source code for the CC2530 devices I haven't been able to do it.  Also, I need this link to be bidirectional.

The design files that I am using can be found here, http://www.ti.com/lit/zip/tidc258,