This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

what does thos code mean of TC_LINKKEY_JOIN

Hi  all

what is the different between disable and enable the TC_LINKKEY_JOIN

i found that when i disable the TC_LINKKEY_JOIN. i could using the long address mode to send the msg ,

it always return ZNwkInvalidRequest ( 0xc2 )




#if !defined OSALMEM_LL_BLKSZ #if defined NONWK #define OSALMEM_LL_BLKSZ (OSALMEM_ROUND(6) + (1 * OSALMEM_HDRSZ)) #else /* * Profiling the sample apps with default settings shows the following long-lived allocations * which should live at the bottom of the small-block bucket so that they are never iterated over * by osal_mem_alloc/free(), nor ever considered for coalescing, etc. This saves significant * run-time throughput (on 8051 SOC if not also MSP). This is dynamic "dead space" and is not * available to the small-block bucket heap. * * Adjust this size accordingly to accomodate application-specific changes including changing the * size of long-lived objects profiled by sample apps and long-lived objects added by application. */ #if defined ZCL_KEY_ESTABLISH_OLD // CBKE no longer uses long lived memory allocations. #define OSALMEM_LL_BLKSZ (OSALMEM_ROUND(526) + (32 * OSALMEM_HDRSZ)) #elif defined TC_LINKKEY_JOIN #define OSALMEM_LL_BLKSZ (OSALMEM_ROUND(454) + (21 * OSALMEM_HDRSZ)) #elif ((defined SECURE) && (SECURE != 0)) #define OSALMEM_LL_BLKSZ (OSALMEM_ROUND(418) + (19 * OSALMEM_HDRSZ)) #else #define OSALMEM_LL_BLKSZ (OSALMEM_ROUND(417) + (19 * OSALMEM_HDRSZ)) #endif #endif #endif