Other Parts Discussed in Thread: Z-STACK
Hi all :
there are two ZR and 40 ZED .
Two ZR were joined the network at first.
and then i add those ZED into the network one by one .
but when i add the 36 , there is a association response “PAN access denied” and i could add any new node ever。
and i try to add a new ZR to enlarge the network, but it also response "PAN access denied".....
1. Is that mean there is not more room for the new node in this network ???
2. when we setup a large network(more than 40 nodes) ,should we adding the ZR first ?
3. if the ZR is power off ,and other ZR and ZC is full of children ,how does those child node will be ?
BR!