Hi all,
I'm facing a problem with the behavior of end devices when they get orphan status. Here's the information I have and the problem:
Info
I have an implementation of multiple networks with different PANID. I started to use different channels for each one, because a beacon request sent in one network, trigger a response from all the possible parents in different networks on the same channel.
Problem
If an end device has never been on a network, its beacons request are only sent to the specific channel seted (OK). But, when it gets an orphan status, the end device sends beacon request to all the channels with every start joining cycle.
I thought this should be related with frequency agility, so I used ZDNWKMGR_MIN_TRANSMISSIONS=20 and ZDNWKMGR_MIN_TRANSMISSIONS=0, but the same result was seen.
Any ideas?
Thanks!