This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: more details of znp and zigbee for beginners

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK,

Hi friends

I have started to working with znp through uart, i have read "Developing a ZigBee® System Using a CC2530-ZNP Approach" and "Z-Stack Monitor and Test API" documents but still don't understand some things and how to set some configs by znp command, i think i need more details of znp commands, as very simple example in " ZB_WRITE_CONFIGURATION -> ZCD_NV_LOGICAL_TYPE" there are 2 bytes i should use to define logical type but i don't know what number should I set to set coordinator and what numbers for router and etc. and ever more details about ZB_WRITE_CONFIGURATION itself, where can i see what does numbers mean and in responses what does each number say! some of them are in z-stack monitor and test document but with very low details!! and my other problem is that i don't understand some general zigbee definitions too, for example I don't know what should i do with app id, device id, NOIC, commissioning cluser ... and how to set them. 

In general I need to make simple zigbee network and i found using host mcu and znp through uart is simple way but i need more details and understanding to try it. what should i read to get more general understanding of main zigbee stuff i need to know to work with znp? i made my own breakout board by cc2530 and mcu, i have connected them and cc2530 znp works properly but i need more understanding than just 3 znp documents.

Regards