Part Number: CC2538DK
Hi everybody!, I'm working in a little proyect of my university that consist in make tests about the energy quality. I have to my disposition these devices:
One-Phase Metrology with Enhanced ESD Protection Reference Design
CC2538 Evaluation Module Kit
I worked succesfully with the TIDM-1PHMTR-ESD, I can read the measures of energy in the display and the GUI in my computer but in order to progress in my proyect I have to send those measures through Zigbee.
I think that I can use the CC2538 as transmitter when it's conected in the TIDM-1PHMTR-ESD (the user guide of the TIDM-1PHMTR-ESD says this but with a CC2530, I'm assuming that I could do the same with the CC2538), and the other CC2538 (maybe conected with the SmartRF06EB) as a reciver.
The user guide says that the CC2530 should be flashed with code to act as a transmitter, so my question is, where I can find that code? I have to program it? If so, exist some kind of tutorial to learn to do it? The user guide of the TIDM-1PHMTR-ESD says that both, the transmitter and the reciver should work in 2.4-GHz, with 115.2 kbaud. I belive that this must be something easy to do, but I can't figure out how to do it. Can someone help me with this? Thank you in advance.