This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531: Not detected by PC after reflashed with Z-Stack

Part Number: CC2531
Other Parts Discussed in Thread: Z-STACK

Hi,

I have purchased three CC2531 USB dongles and a CC Debugger. I want to flash these dongles with Z-Stack (to make them behave as ZigBee) to be able to communicate (send and receive messages) from one ZigBee dongle to another.

I have successfully uploaded the hex file created with IAR workbench and have flashed using the flash programmer. As soon as the flashing is completed, the green light disappeared from the dongle (neither shows the red light). Now if I want to communicate one ZigBee (dongle with Z-Stack) with another, can I do so through USB port? If yes, with which software? Smart RF Studio?

I've tried it with the Smart RF studio but no device shows up when the dongle is connected to a USB port and the Smart RF studio is opened. However, the Smart RF Studio detects SoC CC2531 when the debugger is connected in addition to the dongle.

Reiterating the base question: How to send a message from one dongle to another after uploading Z-Stack on to it?

Looking forward to your answer

Thank you!