I am building a gateway, it use CC2530 +CC2591 ZNP, Z-Stack Home 1.2.2a.44539, I have added the build tag: HAL_PA_LNA.
But it seem the signal not higher. Only the build tag enough or I must modified more to get higher TX/RX?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am building a gateway, it use CC2530 +CC2591 ZNP, Z-Stack Home 1.2.2a.44539, I have added the build tag: HAL_PA_LNA.
But it seem the signal not higher. Only the build tag enough or I must modified more to get higher TX/RX?
Yes, it is the same, I test n SmartRF Studio option range extender, TX power 21dbm and test with sniffer at 10cm far, it show 20dbm in Ubiqua.
But when test with RX option if i enable "High gain mode RX" for cc2591, the signal lower than when i uncheck it.
The module i buy from Webee. You can see the schematic6747.CC2530 PA core board.pdf
cc2630_drop.zipYes, here it is.
It also drop and send beacon request if i bring the cc2630 nearer or father to the ZNP.
As you can see in the log id 261 i turn off the light switch (it is base on sample light) it send the report, now it is about 9 meter away with ZNP.
id 316 bring it near the znp and the problem occure
I have this problem again, i have enable in ZStackCore project :
OAD_KEEP_NV_PAGES NV_RESTORE NV_INIT
But if i let it overnight, it lost connection with ZNP and send beacon request, it is CC2530+CC2591 running ZNP HA 1.2.2.
From what i have read, save and restore network information in CC2630 do in the back ground with Z-stack.
This is strange and occurs with more than 1 device, i have about 10 device running on CC2630 to test, some time it lost connection with ZNP for unknown reason,
After that i must "allow to join " or it could not be control.
Is there any reason NV can lost, or ZNP reject device if they have weak signal? Power not stabilize?
I also have some Xiaomi sensors running in EndDevice mode, and the problem not occurs with those device, it is running NXP chip, one it pair with ZNP, it never lost connection.