Part Number: CC2538DK
Tool/software: TI C/C++ Compiler
CC2538 PER Test (v1.1.0) (Rev. A)
how to generate Rx bin/.out and TX bin/.out file form above package??
I have to put two board on test one is flash with Tx bin file which is continuously transmit, and another board in receive mode which is flash with Rx bin.
Any idea about Rx/Tx bin file??
What changes should i do in per_test.c file ?