Other Parts Discussed in Thread: CC2530, CC2592, Z-STACK
Tool/software: WEBENCH® Design Tools
Hello, I am using CC2530+cc2592 SOC with z-stack 1.0.0 in coordinator. When I start adding device to gateway I can add max 20 devices and work properly. But when I add more devices to it data not reach to gateway at all.
I have changed
#define NWK_MAX_DEVICE_LIST 75 // Maximum number of devices in the Default is 20 in
In nwk_globals.h and
#define INT_HEAP_LEN 2048 // Default is 3072
In OnBoard.h. successfully compiled and download.
But after adding more than 20 devices same thing happened data not reach to gateway.
What is the issue and how I can add more than 50 devices to the gateway successfully.