Hi to everyone,
I have a doubt about how the RAM, ROM, FLASH memory of the device is mapped.
I added some code to the SensorTag stack and in the build phase (Linking phase) I get the following error:
At the end of the SensorTag.map file I see:
44 093 bytes of readonly code memory
2 967 bytes of readonly data memory
772 bytes of readwrite data memory
Errors: 7
Warnings: none
I also attach the "SensorTag.map" file (i just changed the extension from *.map to *.txt).
/cfs-file/__key/communityserver-discussions-components-files/158/SensorTag.txt
Thanks