This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538DK: port openwsn stack code to CC253DK

Part Number: CC2538DK

There has some error when I use the OpenVisualizer to organize the wireless network. If anyone is familiar with OpenWSN stack? It doesn't work after I port the code to CC2538DK.

The slave mote can not identify the EB packet contain the network information sent by the master. It shows:

[IEEE802154E] the received packet format is not supported(code location 3)

[IEEE802154E] the received packet format is not supported(code location 3)

[IEEE802154E] the received packet format is not supported(code location 3)

The error is located at the IEEE80154E.c/isValidEbFormat() funciton. The value of chTemplate_checkpass and slotframelink_ie_checkPass are FLASE, so the function return FALSE and the code is stop.