Other Parts Discussed in Thread: Z-STACK, SIMPLELINK-CC13X2-26X2-SDK
Dear,
Do I can add 3rd party ZED Motion Sensor into Linux Gateway network from Zero Project example ?
If yes, Could you please send me some instruction ?
Thanks,
Khai.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear,
Do I can add 3rd party ZED Motion Sensor into Linux Gateway network from Zero Project example ?
If yes, Could you please send me some instruction ?
Thanks,
Khai.
For Linux Gateway network from Zero Project, you only need to enable permit join and you should read user manual of 3rd party ZED Motion Sensor to know how to make this 3rd party ZED Motion Sensor factory reset to join Zigbee network.
I assume you have referred to the Gateway SLA. Please see this Similar topic. I recommend you confirm operation with the default examples before adding functionality for your motion sensor.
Regards,
Ryan
Dear Ryan, Chen,
1. I already tried Gateway SLA. Project worked with ti znp and zed_light.
2. mMy 3rd zed sensor already went to reset mode but TI gateway can not detect device. I assume 3rd zed have different channel, I'm trying check their channel.
3. I will follow Similar topic as your refer.
Thanks,
Khai.
Dear Chen,
I will setup sniffer follow this instruction : Packet Sniffer. But I saw it support only CC2652, my TI chip is CC2652RB, Can sniffer_fw_15_4.hex firmware work on CC2652RB_LP ?
Dear Ryan, Chen,
I already setup wireshark and Smart RFSniffer 2 follow Packet Sniffer, but I can not get package data from ZED device. I use CC2652RB_LP as sniffer hw tools.
I update info : I already set 3rd temperature zed device goto reset mode. TI Linux gateway discovered and connected with temperature zed successfully. So I make sure wireshark tool can not get package data from zed device.
Thanks,
Khai.
Try to use 3.0.x as it is described in https://dev.ti.com/tirex/explore/node?node=ANbR0LtTwkMnDCiEhygF7A__pTTHBmu__LATEST
Dear Ryan,
Follow your refer topic, I did not understand clearly what I need to do :
1. Link processors.wiki.ti.com/.../Fire_Alarm_System goto Z-Stack project of resource explorer so I didn't what I need to refer. Could you please send me other link.
2. About your comment from 3 year ago : ZNP and gateway resources do not automatically support IAS Zone devices. This is something you will have to include using the ZCL v6 specifications and Fire Alarm examples as a guide" => I found gateway linux didn't support IAS Zone devices, how about ZNP ? Don't It still support same 3 year ago ?
Thanks,
Khai.
Try to refer to https://sunmaysky.blogspot.com/2020/05/how-zigbee-cie-and-ias-device-work.html which shows you what ZC should handle or process when an IAS zone device joins.
The Wiki has been deprecated as of December 2020, but YK has provided his blog post and there are IAS Zone examples provided in the SIMPLELINK-CC13X2-26X2-SDK which you can reference for the necessary Zigbee clusters and attributes. The LINUX-SENSOR-TO-CLOUD gateway solution has not been updated to support IAS devices.
Regards,
Ryan
Dear Chen, Ryan,
I don't check source code yet but I found ZNP device cluster below :
APP/MAIN] PKTBODY: cmdId = NWK_GET_LOCAL_DEVICE_INFO_CNF
[09:52:26.373,536] [SMPLAPP/MAIN] PKTBODY: deviceInfoList :
[09:52:26.373,578] [SMPLAPP/MAIN] PKTBODY: networkAddress = 0x00000000 (0)
[09:52:26.373,623] [SMPLAPP/MAIN] PKTBODY: ieeeAddress = 00:12:4B:00:14:F5:45:26
[09:52:26.373,666] [SMPLAPP/MAIN] PKTBODY: manufacturerId = 0x00000007 (7)
[09:52:26.373,705] [SMPLAPP/MAIN] PKTBODY: simpleDescList :
[09:52:26.373,742] [SMPLAPP/MAIN] PKTBODY: [000] :
[09:52:26.373,780] [SMPLAPP/MAIN] PKTBODY: endpointId = 0x00000004 (4)
[09:52:26.373,821] [SMPLAPP/MAIN] PKTBODY: profileId = 0x00000104 (260)
[09:52:26.373,862] [SMPLAPP/MAIN] PKTBODY: deviceId = 0x00000007 (7)
[09:52:26.373,901] [SMPLAPP/MAIN] PKTBODY: deviceVer = 0x00000000 (0)
[09:52:26.373,940] [SMPLAPP/MAIN] PKTBODY: inputClusters :
[09:52:26.373,978] [SMPLAPP/MAIN] PKTBODY: [000] = 0x00000000 (0)
[09:52:26.374,017] [SMPLAPP/MAIN] PKTBODY: [001] = 0x00000003 (3)
[09:52:26.374,055] [SMPLAPP/MAIN] PKTBODY: [002] = 0x00000501 (1281)
[09:52:26.374,094] [SMPLAPP/MAIN] PKTBODY: outputClusters :
[09:52:26.374,131] [SMPLAPP/MAIN] PKTBODY: [000] = 0x00000006 (6)
[09:52:26.374,169] [SMPLAPP/MAIN] PKTBODY: [001] = 0x00000004 (4)
[09:52:26.374,206] [SMPLAPP/MAIN] PKTBODY: [002] = 0x00000005 (5)
[09:52:26.374,334] [SMPLAPP/MAIN] PKTBODY: [003] = 0x00000500 (1280)
[09:52:26.374,375] [SMPLAPP/MAIN] PKTBODY: [004] = 0x00000009 (9)
[09:52:26.374,415] [SMPLAPP/MAIN] PKTBODY: [005] = 0x00000101 (257)
[09:52:26.374,453] [SMPLAPP/MAIN] PKTBODY: [006] = 0x00000020 (32)
[09:52:26.374,492] [SMPLAPP/MAIN] PKTBODY: [001] :
[09:52:26.374,529] [SMPLAPP/MAIN] PKTBODY: endpointId = 0x000000F2 (242)
[09:52:26.374,570] [SMPLAPP/MAIN] PKTBODY: profileId = 0x0000A1E0 (41440)
[09:52:26.374,609] [SMPLAPP/MAIN] PKTBODY: deviceId = 0x00000061 (97)
[09:52:26.374,650] [SMPLAPP/MAIN] PKTBODY: deviceVer = 0x00000000 (0)
[09:52:26.374,690] [SMPLAPP/MAIN] PKTBODY: outputClusters :
[09:52:26.374,728] [SMPLAPP/MAIN] PKTBODY: [000] = 0x00000021 (33)
[09:52:26.374,770] [SMPLAPP/MAIN] PKTBODY: deviceStatus = DEVICE_ON_LINE
Cluster 0x501 & 0x500 is IAS ACE and IAS ZONE, so it mean new ZNP source already support IAS ZONE, do I understand correctly ?
Thanks,
Khai.
ZNP doesn't support ZCL part. ZCL is implemented on ZNP host instead of ZNP itself.
Dear Chen, Ryan,
Linux Gateway application already connect to 3rd temperature sensor and door sensor as picture below :
I have some question :
1. After connecting to temperature sensor, temperature will report temperature value each 5 minutes => I checked and didn't see any setup for this feature so it is default feature of ZED ?
2. When door sensor on/off, door sensor zed reported to gateway success but I didn't see linux gateway application received any report package => Do I miss something ? why gateway can auto receive report from temperature sensor but can not receive report from door sensor ?
Thanks,
Khai.
1. If you don't so report configuration from gateway, it might be default value of your ZED. You should check user manual of your 3rd party device.
2. Do you add CIE support in your Linux GW? If not, your GW might not be able to receive IAS zone state notification/report.
Dear Chen,
Thank for your reply.
Do you add CIE support in your Linux GW? If not, your GW might not be able to receive IAS zone state notification/report => But GW can receive report from temperature ZED, what's different between 2 report type ?
Thanks,
Khai.
As I know, TI Z-Stack Linux GW implements ZCL temperature cluster support by default so you can see temperature sensor work by default. However, CIE is not implemented by Z-Stack Linux GW reference design so you have to add it by yourself.
"TI Z-Stack Linux GW implements ZCL temperature cluster support by default" => Was This feature be implemented at Linux GW Application or ZNP CC2652RB ?
When I check sniffer tool, ZNP CC2652RB can receive report package from door sensor (as picture I sent) but GW application don't receive any package from ZNP CC2652RP, I think package was filtered by ZNP CC2652RP. Do I understand correctly ?
I had replied you ZCL is implemented on Host instead of ZNP so the ZCL temperature cluster support is implemented on Linux GW application.
Dear Chen,
ZCL is implemented on Host instead of ZNP so the ZCL temperature cluster support is implemented on Linux GW application => I already print out raw message what ZNP send to GW application. I didn't see any raw package when ZED send report attribute, so I make sure ZNP didn't forward report package to GW application.
When 3rd ZED door sensor send report attribute to GW, I didn't see APS package return from GW (picture below), I guess that why GW App can receive report attribute package => Do I miss something ?
Do you can show me ZNP functions where handling package from ZED (Ex : response APS ack to ZED, or filter package from ZED).
Thanks,
Khai.
I would suggest you to use sniffer to check the process of temperature sensor joining process and how it report temperature instead of checking ZNP raw message.
In the ZNP firmware, once an endpoint has been registered locally then an application will be notified of any received data as an AF Incoming Data Indication through an OsalPort message. You can check MT_ProcessIncomingCommand -> case AF_INCOMING_MSG_CMD -> MT_AfIncomingMsg. The host gateway application example only handles incoming temperature measurement reports by default in zb-gateway.js:
// #################### Device Report - Incoming Report #################################### .on('hagateway:gw:report', function(data){ // read incoming report based on what its ClusterID is switch(data.clusterId){ // incoming temperature measurement case ZBL.HA_CLUSTER_ID.TEMPERATURE_MEASUREMENT: if( (data.attributeRecordList[0].attributeId === ZBL.TEMPERATURE_MEASUREMENT_CLUSTER.MeasuredValue) && (data.attributeRecordList[0].attributeType === ZBL.DATA_TYPE.INT16)) { var raw_temp = data.attributeRecordList[0].attributeValue; raw_temp_string = reverse(raw_temp).toString('hex'); raw_temp_int = parseInt(raw_temp_string, 16); var temp = raw_temp_int / 100; console.log("Zb-Gateway: The temp is: ", temp); var temp_data = { guid: data.guid, temp: temp }; ZigbeeGatewayInstance.emit('zb-gateway:temp_device:temp', temp_data); } break; } })
Regards,
Ryan
Dear Ryan, Chen,
I found out somethng wrong about report package endpoint destination. In picture below, destination endpoint is 2 but gw ep is 4, so I guest that cause report was rejected. Do you know how this happen ?
Note : I used TI ZED light on CC2652RB and configed report onoff attribute => TI ZED light already send report each 30 seconds but ZNP did not forward report to GW applicaiton.
Thanks,
Khai.
In your sniffer log, the destination endpoint of binding request is set to endpoint 2.
Dear Chen,
Thanks you, GW received report successfully.
Just notify where I got problem is : "gateway_self_addr.endpoint = GATEWAY_MANAGEMENT_ENDPOINT" with GATEWAY_MANAGEMENT_ENDPOINT = 0x2 in default source.
Thanks,
Khai.
GATEWAY_MANAGEMENT_ENDPOINT should not have any effect on your application, are you saying that it needed to be changed in order for you to receive reports from your devices?
Regards,
Ryan
Dear Ryan,
I used global variable "gateway_self_add" in my function. As I comment above GATEWAY_MANAGEMENT_ENDPOINT = 0x2 but gateway ep id was config at gateway_config.tlg file, by default, gatway ep id in the config file is 0x4.