This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2533 vs CC2530, how compatible are these?

Part Number: CC2530
Other Parts Discussed in Thread: CC2533,

Dear champs,

My customer uses CC2533 in an existing product today, but looking to use CC2530 in some products. How compatible are these?

Pinouts are very similar apart from pins 1-4 which are unused on CC2530 and should be connected GND according to datasheet. Is this mandatory, i.e. are these pins connected to die GND or just floating inside the package? Customer is asking for layout reuse purposes.

Other differences are obvoius from the datasheets, such as flash sizes, Rx sensitivity and Tx output power.

Thanks,

/ Wolfgang