Part Number: CC2652P7 Other Parts Discussed in Thread: CC2674P10 , CC2652P , CC2530 , Z-STACK Tool/software: Hello
Feasibility Analysis: 500 Powered Devices in a 3m×5m Room Using Zigbee Communication to Transmit Status Within 20 Seconds
Configuration…
Part Number: CC2652P7 Other Parts Discussed in Thread: SYSCONFIG , CC1352P7 , CC2652R7 Tool/software: Hello,
i tried to build and use the ot-ti ( https://github.com/TexasInstruments/ot-ti ) Firmware for an RF-BM-2652P4 CC2652P7. I cloned the repository…
Part Number: CC2652P7 Tool/software: Hi everybody, I am really frustrated right now, because my custom layout does not work as intended. What I have did was copying the hardware guide (I know its not the best solution, but for me its the only one for…
Part Number: CC2652P7 Tool/software: Does the IEEE 802.15.4 interface comply with the generic requirements of a PHY DSSS O-PQSK operating in the 2450 MHz band in accordance with the IEEE 802.15.4 standard?
Part Number: CC2652P7 Other Parts Discussed in Thread: CC2652P Tool/software: I am trying to integrate OTBR running on ESP32 with Thread firmware on CC2652P/P7/P10. Thread firmware is based off the 1.3 certified release from last year. This OTBR implementation…
Part Number: CC2652P7 Other Parts Discussed in Thread: Z-STACK Tool/software: Hai,
We developed the Zigbee coordinator based on cc2652p7 chip with the software of ZNP and its working.
Now we are planning to implement the Backup feature, my setup is…
Part Number: CC2652P7 Tool/software: Hi,
Customer is doing stability test, fast temp change between -40~85.
Zigbee protocol. ZR role.
if 30s network sync, the device's RF has issue to communicate. looks the PLL is unlocked based on the snapshot…
Part Number: CC2652P7 Other Parts Discussed in Thread: CC2652P , Z-STACK Tool/software: Hi Team,
Please help to review the CC2652P schematic file.
This design uses a shared antenna for BT and Zigbee. Please help confirm the following questions: 1…
Part Number: LP-CC2652RB Other Parts Discussed in Thread: CC2652RB Tool/software: hey there, I am back to this party after a longer break.. this was the original thread: https://e2e.ti.com/support/wireless-connectivity/zigbee-thread-group/zigbee-and-thread…
Part Number: CC2652P Other Parts Discussed in Thread: CC2674P10 Tool/software: Hi Expert,
My customer's application is wifi router + thread repeater. I think that NCP can maintain thread connection when wifi soc goes to sleep mode.
CC2652P7 can do…
Part Number: CC2652P Other Parts Discussed in Thread: CC1352P , , Z-STACK , CC2652R7 , , SYSCONFIG Tool/software: Hai,
We are planning to make a Zigbee gateway with CC2652P as a ZigBee coordinator (ZNP) and esp32 will communicate using UART with ZNP…
Part Number: CC2652P7 Hai,
We are designed a gateway which have ZigBee coordinator (ZNP-APP) chip as CC2652P7.
I'm having doubt on the antenna section, we referred the two Launchpad schematics LP-CC1352-P2 and LP-CC1352P7-4. Both are having different…
Part Number: LP-CC1352P7 Other Parts Discussed in Thread: CC2652P7 , CC1352P7 I am building Openthread RCP example from Simplelink 7.10.02.23 for LP_CC1352P7-4 board, however having trouble when I set the baudrate to 460800. On starting otbr-agent it…
Part Number: CC2652P7 Other Parts Discussed in Thread: CC2652P We now have a door lock device using cc2652p and the protocol stack is simplelink_cc13x2_26x2_sdk_5_10_00_48. The door lock can be added to our private gateway normally, and the private gateway…
Part Number: CC2652P7
Hello,
I am using a custom designed board based on CC2652P7 chip.
SDK used: simplelink_cc13xx_cc26xx_sdk_7_10_00_98
API used: UART2_write(uart, data, len,&bytesWritten);
The data printed on serial terminal is incomplete…
Part Number: CC2652P7 Other Parts Discussed in Thread: SYSCONFIG I have flow this course Matter Device Creation — CC13XX CC26XX SimpleLink Academy and installed developing condition on ubuntu.
But when execute "gn gen out/debug --args = "ti_sysconfig_root…
Part Number: SIMPLELINK-CC13X2-26X2-SDK Other Parts Discussed in Thread: Z-STACK , ARM-CGT , CC2652RB , SYSCONFIG , CC2652P , CC2652P7 , CC1352P With recent SDKs, many users a reporting stability issues (total crash, mac errors, nwk table full errors…
Part Number: LP-CC1352P7 Other Parts Discussed in Thread: CC1352P7 , CC2652P7 , Z-STACK , SYSCONFIG
I loaded the ZR_SW_LP_CC1352P7_4_tirtos7_ticlang.out from the example simplelink examples (a zigbee router node) on the LP. trace_ti_router_sonoff_coordinator…
Part Number: CC2652P7 Hi,
I need to use log functions in my algorithms(ex: log10f) and also to print floating point numbers.
Have included " #include <math.h>"
Looks like the compiler is not able to find math.h. I don't get any build errors though…
Part Number: CC2652P7 Hi,
I have an application that runs a state machine in a loop.
I want to soft reset the chip based on UART command from a terminal asynchronously.
How can I do that?
Thanks
Karthik
Part Number: CC2652P7 Other Parts Discussed in Thread: CC1352P7 , Z-STACK Good morning,
We are working on custom board with CC2652P7 as coordinator, based on LP-CC1352P7-4 design without sub-GHz part. Antenna switch SKY13317 (3 ways) is replaced by…
Part Number: CC2652P7 Other Parts Discussed in Thread: CC1352P7 A customer is trying to commission a GPD to zc_thermostat_sink running on CC1352P7, but found that the GPS did not response to the channel request from GPD.
After single stepping into the…