Other Parts Discussed in Thread: MSP430F5529, CC2564
We’ve got a TI MSP430F5529 experimenter board and a CC2564 Bluetooth chip. We’ve used the SPPLEDemo_Lite and have gotten it to work.
We are now trying to get it to work on our board. Again, we’ve got the 5529 and the CC2564 chip hooked up with our 4 lines (TX, RX, CTS, and RTS) hooked up (each flipping into the other’s counterpart as shown in the diagrams). We get to the BCS_Initialization and it returns with –4.
In Debug during HCITR_COMOpen, we can watch RTS go high and CTS go low. After that, we never see traffic on these lines or the RX and TX lines.
Any advise would be great
Update: We decided to watch the RX and TX lines. The TX line sends some data and the RX line then sends some data. This happens once then BSC_Initialize returns -4. Upon closer inspection, the RTS and CTS do alter during this event.