Hi,
i'm using two system based on STM32F4, CC2564B in order to test HFP. One side is HandsFree Server (called OpenHFServer), the other HF client (called OpenRemoteHandsfreePort).
The problem is that Service Level Connection is not opened due to a connection stall.
Open Port Indication (on the Server Side) and Open Port Confirmation (on the client Side) are received by the SS1 (v 4.0.2.2) stack as events from CC2564B.
By debugging on the client side, i see that there is an LMP_set_AFH message repeated that blocks the connection...
How can I solve this issue?
Here in attachment there are the connection logs:
Thanks in advance
Best Regards,
Paolo