Other Parts Discussed in Thread: CC2540
Hi,
I'm having some trouble getting the CC2540 USB dongle to work with BTool. I'm following the instructions in this document http://www.ti.com/lit/ug/swru301a/swru301a.pdf, but the driver shows up not as a serial port, but in the "Cebal controlled devices" section, with no Port indicated.
I have tried manually updating the drivers to the ones provided in C:\Program Files (x86)\Texas Instruments\BLE-CC2540-1.1a\Accessories\Drivers, however I get an error message reading: "The folder you specified doesn't contain a compatible software driver for your device. If the folder contains a driver, make sure it is designed to work with Windows for x64-based systems".
When launching BTool I am greeted with the following error before the UI finishes initializing:
See the end of this message for details on invoking
just-in-time (JIT) debugging instead of this dialog box.
************** Exception Text **************
System.InvalidOperationException: Failed to compare two elements in the array. ---> System.FormatException: Input string was not in a correct format.
at System.Number.StringToNumber(String str, NumberStyles options, NumberBuffer& number, NumberFormatInfo info, Boolean parseDecimal)
at System.Number.ParseInt32(String s, NumberStyles style, NumberFormatInfo info)
at BTool.CommSelectForm.<SortComPorts>b__0(String strA, String strB)
at System.Array.FunctorComparer`1.Compare(T x, T y)
at System.Collections.Generic.ArraySortHelper`1.SwapIfGreaterWithItems(T[] keys, IComparer`1 comparer, Int32 a, Int32 b)
at System.Collections.Generic.ArraySortHelper`1.QuickSort(T[] keys, Int32 left, Int32 right, IComparer`1 comparer)
at System.Collections.Generic.GenericArraySortHelper`1.Sort(T[] keys, Int32 index, Int32 length, IComparer`1 comparer)
--- End of inner exception stack trace ---
at System.Collections.Generic.GenericArraySortHelper`1.Sort(T[] keys, Int32 index, Int32 length, IComparer`1 comparer)
at System.Array.Sort[T](T[] array, Int32 index, Int32 length, IComparer`1 comparer)
at System.Array.Sort[T](T[] array, IComparer`1 comparer)
at System.Array.Sort[T](T[] array, Comparison`1 comparison)
at BTool.CommSelectForm.SortComPorts(String[] rgstrPorts)
at BTool.CommSelectForm.commSelect_FormLoad(Object sender, EventArgs e)
at System.Windows.Forms.Form.OnLoad(EventArgs e)
at System.Windows.Forms.Control.CreateControl(Boolean fIgnoreVisible)
at System.Windows.Forms.Control.CreateControl()
at System.Windows.Forms.Control.WmShowWindow(Message& m)
at System.Windows.Forms.Control.WndProc(Message& m)
at System.Windows.Forms.Control.ControlNativeWindow.WndProc(Message& m)
at System.Windows.Forms.NativeWindow.Callback(IntPtr hWnd, Int32 msg, IntPtr wparam, IntPtr lparam)
************** Loaded Assemblies **************
mscorlib
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5448 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/Microsoft.NET/Framework64/v2.0.50727/mscorlib.dll
----------------------------------------
BTool
Assembly Version: 1.0.0.0
Win32 Version: 1.0.0.0
CodeBase: file:///C:/Program%20Files%20(x86)/Texas%20Instruments/BLE-CC2540-1.1a/Projects/BTool/BTool.exe
----------------------------------------
System.Windows.Forms
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5446 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Windows.Forms/2.0.0.0__b77a5c561934e089/System.Windows.Forms.dll
----------------------------------------
System
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5447 (Win7SP1GDR.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System/2.0.0.0__b77a5c561934e089/System.dll
----------------------------------------
System.Drawing
Assembly Version: 2.0.0.0
Win32 Version: 2.0.50727.5420 (Win7SP1.050727-5400)
CodeBase: file:///C:/Windows/assembly/GAC_MSIL/System.Drawing/2.0.0.0__b03f5f7f11d50a3a/System.Drawing.dll
----------------------------------------
************** JIT Debugging **************
To enable just-in-time (JIT) debugging, the .config file for this
application or computer (machine.config) must have the
jitDebugging value set in the system.windows.forms section.
The application must also be compiled with debugging
enabled.
For example:
<configuration>
<system.windows.forms jitDebugging="true" />
</configuration>
When JIT debugging is enabled, any unhandled exception
will be sent to the JIT debugger registered on the computer
rather than be handled by this dialog box.
If I am using the incorrect driver, where can I get a correct one for Windows 7?
If the driver is correct, how do I go about resolving the BTool exception on startup?
Thanks and best regards,
Jan