Other Parts Discussed in Thread: CC2541
Hi everyone,
I've got an issue with the power consumption of the CC2541. The situation is as follows: I've got a custom PCB which is derived from a perfectly working board (with only slight differences of the schematics). On the new board, the CC draws about 500µA current, even in sleep mode. If I put exactly this CC onto the old board, this current offset is gone. If I solder it back onto the new board the offset is measurable again. I verified this with at least 3 CC chips. The new board without the CC shows no current draw so it has no built-in short circuits.
Except for this current offset the new board is performing very well with good RF performance. So I guess this is not a problem.
Unused peripherals (I²C, ADC input) are not connected and not in use. The problem occurs with the original TI stack (1.2.1) and with my custom firmware.
Any ideas what might cause the CC to draw that much current in sleep mode? Your help is much appreciated.
Best Regards,
Philipp