Dear all:
I downloaded MasterSlaveSW in TI's Wiki ,and then adding UART which I used HAL's API,sellecting DMA .However, the following hapens .
Error[e104]: Failed to fit all segments into specified ranges. Problem discovered in segment XDATA_N. Unable to place 2 block(s) (0xc02 byte(s) total) in .0xa13 byte(s) of memory. The problem occurred while processing the segment placement command "-P(XDATA)XDATA_N=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were "XDATA:14ed-1eff"
I was writing IAR sometimes encounting a problem. About BLE4.0,
These paragraph in literal is not enough memory.
the XDATA: 14ed-1eff (2578 bytes), but 2 block (s) (, 0xc02 byte (s) total)(3047bytes),so it doesn't fit it memory.
Does everybody has the experience in this field? I want to ask everybody how to solve this part?
I would be very grateful.
thanks !