This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541 Logic Levels @ VDD = 2.5V.

Other Parts Discussed in Thread: CC2541

We are prototyping with the BLE CC2541. I need to know what the Logic-1 input voltage with VDD = 2.5V (regulated down from an LIR). I'm reading external I/Os that vary with the unregulated battery voltage and need to know the range that will register as a hi.  I'm having a hard time tracking down the DC Characteristics when powered at VDD = 2.5V -> the datasheet only has DC characteristics at 3V. Any know the answer or dealt with this? I have to imagine that the logic levels are well defined over the voltage range of 2 - 3.6V.

Thanks - JP