Other Parts Discussed in Thread: CC2540
Hello,
In my central code i have kept following connection parameters
Min connection interval = 100 ms
Max. connection interval = 100 ms
slave latency = 0
supervision timeout = 3 second
sometimes my central devices disconnects immediately after connecting to peripheral device.
I checked the error for disconnection and it is "LL_STATUS_ERROR_CONNECTION_TIMEOUT"
Peripheral's default connection are also 100 ms so what can be the reason for disconnection ?
Any help would be highly appreciated.
Thanks,
Smitesh mali