Other Parts Discussed in Thread: CC2540, CC1101
Hi,
I am facing with CC debugger and some BLE112 modules (with the CC2540 inside).
Is any configuration needed to allow modules (are factory default) being recognized by CC debugger?
I always get the RED led. never the green one.
I am following the 6 connections described below:
Pin of debugger--Name-----BLE_pin
1----------------------GND--------GND
2----------------------VDD--------AVDD
3----------------------DC----------P2.2
4----------------------DD----------P2.1
7----------------------RESET-----RES
9----------------------VDD--------AVDD
CC debugger is recognized by BLE update and FLASH programmer, but not the target I want to program (the BLE112)
I also updated CC debugger to last firmware version (0041).
What am I doing wrong?
I can post a photo if needed.
Thanks in advance.