Other Parts Discussed in Thread: CC2541, TPS62730
Hi
I am using cc2541 together with tps62730 for minimum power consumption. I would also like to use a gpio pin (configured as output) as power supply to my other sensors (consuming approximately 0.5 ma). What I am wondering about is what the voltage of an output pin in high state will be when Vdd is 2.1V.
In the cc2541 data-sheet in the DC CHARACTERISTICS section it is stated that Logic-1 output voltage on 4-mA pins will be minimum 2.4V when Vdd is 3.0 volt. What will be the output voltage be when Vdd is 2.1 V (output from tps62730).
Regards Arne