I purchased the Debugger DevPack in hopes that I could use it for both debugging and as a convenient way to prototype additional hardware connected to the SensorTag using the unpopulated pcb header included on the Debugger DevPack PCB.
I want the Sensortag to work when there is no USB connection to the Debuger DevPack.
It is working as a debugger, but unfortunately when I unplug the USB cable, the SensorTag does not run.
Is it held in reset or something? Is there a way around this? (hardware modification?)
If not, is there a blank prototyping DevPack with just a breakout connection to IO pins and some proto-board space?