Hello,
Background:
We have been running the CC2650EM 7ID using the RF06 evaluation board with CCS V6. Our target device is being switched to a CC2640 with a 5x5 mm package from the 7x7mm. So we want to test our BLE program using the CC2650EM 5XD prior to porting to the new PCB. The SimpleBLEPeripheral app was used as a starter, and to also build and test a new iOs application. The design provides a virtual wire for the UART plus some sensor data.
I recently purchased a CC2650EM 5XD to test the code on the 5x5 mm chip to make sure it is ready to port to the new pcb. I didn't have success getting the SimpleBLEPeripheral to run on our target pcb.
Questions:
1) What do I need to change in the Project Settings to build and debug the CC2650EM 5XD? Project runs fine with the CC2650EM 7ID.
a. Change Board.c & Board.h files by using preprocessor define CC2650EM_5XD, and including path to the board.c/.h files for the CC2650EM_5XD
b. Disable LCD support by not defining TI_LCD_INLUDED.
2) Do I need to purchase a License for CCS V6 to run our external target using the SmartRF06 via XDS100v3?
Thanks for your help!
Dan