Other Parts Discussed in Thread: CC2540, CC2541, CC2650, CC2640
Hi everyone,
1º) I am trying to make an apllication that allows to send parameters from the mobile phone to the cc2540 chip via BLE, but I am quite new to these kind of issues. Can you tell me if there is any sample project available that allow me to connect the mobile with the cc2540(as "simple" as that)? Some references to have information about the kind of message that I should listen to or similar?
2º) When I receive the parameters from the mobile phone I have to send it through UART. I am using the SmartRF05 EB and debugging the cc2540 externally through the P18 and P20 modules, dedicated for Debug connectors. Any project which help me to do that?
Thanks in advance for your attention,
Miguel