Other Parts Discussed in Thread: CC2540, CC2650
I'm using matlab to developp some application with ti-sensortag and cc2540 bluetooth dongle and my work is based on : https://github.com/sid5291/SensorTag-Matlab, and BleHealth Demo
so, the connection between matlab and the sensortag is established and i can send and recive data correctly, the broblem is that im using a loop (while(1)) to read data from accelerometer, for each iteration in the loop i open the serial port, send commande and recive data, those operation take a long time (1 s for each iteration) so i'm asking if there is ather solution to get data faster and plot the in real time (like demo blehealth )
there is my code, if any one can help me to modify it to be more faster and to skip all warning in matlab:
clear all
close all
clf
% HCI_TXRX used to send and recive data from serial port
function [result] = HCI_TXRX(data,type)
ADDRESS_TYPE = 1;
if(nargin < 2)
type = 0;
end
s = serial('COM3');
set(s,'BaudRate',115200,'Timeout',0.2,'FlowControl','none','Parity','none');
dec=hex2dec(data);
fopen(s);
fwrite(s,char(dec)');
if(type == 1)
temp_h = dec2hex(0,2);
i = 1;
while (1)
temp = fread(s,1);
if(isempty(temp))
continue;
end
temp_h = [temp_h; dec2hex(temp,2)];
i =i+1;
if(strcmp(temp_h(i-1,:),'01') && strcmp(temp_h(i,:),'06'))% Discovery Done
break;
end
end
end
tic;
while(toc < 2)
end
[A,count] = fread(s);
fclose(s);
h=dec2hex(A);
if(type==1)
h = [temp_h;h];
end
%disp('Raw Data:')
%Hex_disp(h);
i = 1;
while(i<=length(h))
if(h(i,:) == '04')
data_length = hex2dec(h(i+2,:));
i = i+3;
payload = h(i:(data_length+i-1),:);
i = i + (data_length-1);
%disp('Payload:')
%Hex_disp(payload);
if(payload(3,:) == '00')
% disp('Success')
if(type == 1)
if(strcmp(payload(1,:),'01') && strcmp(payload(2,:),'06')) % Discovery Done
% disp('Discovery Done')
devices = hex2dec(payload(4,:));
% fprintf('Number of Devices %d\n',devices);
% disp('Addresses');
size = length(payload);
for m = 1:devices
address = payload(size-5:size,:); % 6 byte MAC Address
% fprintf('Device %d MAC Address(reversed):\n',m);
% Hex_disp(address,ADDRESS_TYPE)
size = size - 8;
end
end
elseif(type == 4)
if(strcmp(payload(1,:),'0B') &&strcmp(payload(2,:),'05')) % GATT_ReadRsp
result = payload((length(payload)-3):length(payload),:);
%disp('Raw Result')
%disp(result)
end
end
elseif(payload(3,:)== '12')
disp('Not in Correct State')
elseif(payload(3,:) == '11')
disp('Already Performing task')
else
disp ('Error')
end
end
i=i+1;
end
end
% function Hex_disp is used to display data
function Hex_disp(data,type)
if(nargin < 2)
type = 0;
end
h_disp = ' ';
for i=1:length(data)
if(type == 0)
h_disp=[h_disp data(i,:) ' '];
elseif(type == 1)
h_disp=[h_disp data(i,:) ':'];
end
end
disp(h_disp);
end
% main script :
GAP_initialise=['01';'00';'FE';'26';'08';'05';'00';'00';'00';'00';'00';'00';'00'
'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'00'
'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'00';'01'
'00';'00';'00'];
GAP_DeviceDiscovery = ['01';'04';'FE';'03';'03';'01';'00'];
SCAN_TYPE = 1;
GAP_connect = ['01'; '09'; 'FE'; '09'; '00'; '00'; '00' ;'52';'DE'; 'AB' ;'29' ;'6A' ;'BC']; %BC:6A:29:AC:50:46 (1325 Tag)
CONNECT_TYPE = 2;
% Reference processors.wiki.ti.com/.../BLE_SensorTag_GATT_Server.pdf
% 0x31 is the address of the acceloremeter config in the GATT server
GATT_AccOn = ['01'; '92'; 'FD'; '05'; '00'; '00'; '31'; '00'; '01'];
GATT_AccOff = ['01'; '92'; 'FD'; '05'; '00'; '00'; '31'; '00'; '00'];
% 0x31 is the address of the acceloremeter config in the GATT server
GATT_AccPerMin = ['01'; '92'; 'FD'; '05'; '00'; '00'; '34'; '00'; '0A'];
GATT_AccNoti = ['01'; '92'; 'FD'; '05'; '00'; '00'; '2E'; '00'; '01'];
WRITE_TYPE = 3;
% 0x2D is the address used to read the acceloremeter data in the GATT server
GATT_AccRd = ['01'; '8A'; 'FD'; '04'; '00'; '00'; '2D' ;'00' ];
READ_TYPE = 4;
disp('Going to Intialize');
HCI_TXRX(GAP_initialise);
disp('Going to Scan');
disp('Make Sure Led D1 is blinking on Sensor Tag');
disp('Wait for Scan To End');
input('Press any key to continue');
HCI_TXRX(GAP_DeviceDiscovery,SCAN_TYPE);
disp('Going to Connect to Sensor Tag');
disp('LED D1 will turn off when Connected, if doesnt there is an error');
HCI_TXRX(GAP_connect,CONNECT_TYPE);
disp('Going to Turn On Acc');
HCI_TXRX(GATT_AccOn,WRITE_TYPE);
HCI_TXRX(GATT_AccPerMin,WRITE_TYPE);
% HCI_TXRX(GATT_AccNoti,WRITE_TYPE);
disp('Going to Turn On Accelerometer');
i =1;
clf
while(1)
result = HCI_TXRX(GATT_AccRd,READ_TYPE);
% result(1,:) is not used (data from acc x:y:z 3 bytes )
rawval = hex2dec([result(2,:); result(3,:); result(4,:)]);
xval = rawval(1)/64; % calculate acc, unit g, range -2, +2
yval = rawval(2)/64;
zval = rawval(3)/64;
% show data
fprintf('Acc X: %f \n',xval);
fprintf('Acc Y: %f \n',yval);
fprintf('Acc Z: %f \n',zval);
%char = input('Press any key to continue (x to exit)','s');
% read 10 sample from accerometer
if(i == 100)
break;
end
% update table of samples
graphe_x(i) = xval;
graphe_y(i) = yval;
graphe_z(i) = zval;
% update graph with new samples
figure(1), plot(graphe_x,'r'), hold on
plot(graphe_y,'g'), hold on
plot(graphe_z,'b')
% increment counter
i = i + 1;
end